Post Go back to editing

output impedance of Vcm

Thread Summary

The user asked about the output impedance of Vcm0 for the AD3551R when used with a fully differential amplifier ADA4945. The final answer indicates that the output impedance of Vcm0 is not specified in the datasheet, but suggests using the evaluation board schematic from the EVAL-AD3552R user guide, which includes a provision for a 0.1uF capacitor for Vcmx in more demanding applications. The user also referenced a technical article on using differential I/O amplifiers in single-ended applications, which provided a useful configuration.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD3551R

  I was wondering if you could tell me the effective output impedance of Vcm0 (the Common-Mode Voltage for DAC0 External TIA)?  The data sheet states that the output impedance of the reference output is quite low (50 mOhms) but I did not find any mention of the output impedance of Vcm0.

  I am asking because I am using the AD3551R with a fully differential (input/output) amplifier ADA4945, and I initially included a feedback RC on the +FB (to the Vcm0, connected to IN-); I think this was a mistake, but I thought that it should not matter if Vcm0 had a low output impedance.  I tried to simulate the setup, but I needed to include about a 10 kOhm ouput impedance for Vcm0 to match measurements.  (specifically, with a 3.2 kOhm / 220 pF feedback, I was seeing a 2.4 V differential dc offset).

  (I am now doing something very similar to figure 3 of https://www.analog.com/en/resources/technical-articles/using-a-differential-io-amplifier-in-single-ended-applications.html , which seems to work as expected.)

Thank you for your help,

Nathan

Thread Notes

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.