Post Go back to editing

Issue with AD5700 recognizing the start bits of Preamble

Category: Hardware
Product Number: AD5700-1

AD5700 is struggling to recognize the start Bits.

 

This is the Oscilloscope, note there is a bit of delay before HART modem starts translating data.

(Blue is RTS Line and it confirms that RTS line is working fine and i also probed CD pin and starts just before the data translation i.e. it skips the preamble)

 

I also checked the timing of one of the initial Zero at the start "0 / 2200Hz" which should have been enough to signal data start -  

And this is 833uS which is good. It is not a DC Bias Issue as i looked at the Waveforms and i do not see any weird Bias anywhere.

 

I tried probing at the input of ADC_IP as well Just to check in case their is some miscommunication after the bandpass filter but NO, Hart signal is alright at this point as well. 

Do you guys have any idea as to why this delay might be happening. I can see other people have also asked this question but couldn't find any applicable answer.

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.