Post Go back to editing

TIDA-01573: RF to Optical Conversion Scheme

Category: Hardware
Product Number: ADN8810

Below is my requirement of RF Signal Transmission on Fiber

  1. Core Function

    • Transmit 100MHz RF signals over 1550nm optical fiber

    • 2mW optical output power with ±5% stability

  2. Key Constraints

    • No bias tee: Direct RF+DC summing on PCB is preferable than any external summing module

    • No TEC: Passive thermal management only, application doesnt require one

    • Single PCB solution: Fully integrated design, most preferablly

Is there any solution done like this from ADI , i could not find any reference design also 

I was sucessful in designing RF Rx and TTL Rx, and TTL Tx with help of ADI solutions and complete analog chain, but sending RF over Fiber is little tricky part i am stuck and need some reference

NOTE: Here the signal is RF not a TTL or LVDS like in most reference designs i see are around LIDAR or Optical Gbpgs Transmitters

Thread Notes

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.