Post Go back to editing

Is there a model or formula that can describe the output value of a DAC?

Thread Summary

The user observed nonlinearity in the output of the MAX538ACSA+ DAC, particularly at low data codes, which is attributed to a zero-code deadband. The datasheet specifies linearity from code 11 upward, and the user can improve accuracy by ignoring lower codes or applying open-loop calibration techniques. The user also noted periodic errors with Tminor = 64 and Tmajor = 256, suggesting a consistent internal pattern that may be modeled for further correction.
AI Generated Content
Category: Hardware
Product Number: max538acsa, max538

Hi, I used a multimeter (with 10 μV accuracy) to record the output of a DAC (PN: MAX538ACSA+), and compared the actual values with the theoretical ones. I found that when the data code is relatively small, the ratio (actual/theoretical) is much lower. Around a data code of 500, the ratio approaches 0.999. Is this normal? Is there a model or formula that can describe this variation so that I can accurately determine the DAC's output value? Thanks.

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.