Category: Hardware
Hello,
With an FTDI module FT4232H , I send SPI command but for code under 0x4000 Voutput value is different from datasheet .I use CSn from SPI tie to sync\
12 bits => 4 first LSB are unused.
gain 1
Vref interne 2.5V
Vlogic 3.3V
VDD 5V
Vout (code=0xFFFF) = 2,500V
Vout (code=0xC000) = 1,875V
Vout (code=0x8000) = 1,25V
Vout (code=0x7FF0) = 2,500V
Vout (code=0x4000) = 1,875V
Vout (code=0x2220) = 1,000V
Vout (code=0x0010) = 0,002V


Someone have an idea, thanks for your help.