Post Go back to editing

Reset for AD5592RBCBZ-1-RL7

Category: Hardware
Product Number: AD5592RBCBZ-1-RL7

I’m planning to use the AD5592RBCBZ-1-RL7 in my design, with Vlogic at 1.8V and VDD at 3.3V. Since the AD5592RBCBZ-1-RL7 doesn’t have a dedicated reset pin, how can we reset the SPI bus if we encounter any issues with SPI communication?

I understand that the AD5592RBCBZ-1-RL7 has an internal reset command via the SPI bus. However, how can we reset the device if we face issues with the SPI bus itself while using the AD5592RBCBZ-1-RL7?

Thread Notes