HI Engineer Zone Team
I am using the LTC2662 in the DC2692A demo board with QuickEval and DC2026C Linduiono.
The LTC2662 functions as as expected all the ranges except the 0-200mA and 0-300mA ranges.
The DAC output current is half the set value in the 200mA span and one third the set value in the 300mA span.
This is if the required output is set to 100mA in the 200mA span I get 50mA output and it is consistently half throughout the entire 200mA range.
Similarly if the required output is set to 240mA in the 300mA span I get 80mA output and it is consistently one third throughout the entire 300mA range.
I have tried it in the setup where DC2026C with DC590 emulator firmware and also where the DC2026C controlled by the sketch.
In both cases the result is the same.
I aware of the incorrect span value mentioned in the post "LTC2662-16 the 300mA Span doesn't work".
I have corrected this but still the same behaviour.
My setup has the following parameters.
V+ = +15V, V- = GND = 0V. Reference Internal = 1.25V,
FSADJ is tied to VCC, an internal RFSADJ (20 kΩ) is selected and hence nominal output range.
Output load is a Fluke 87 III multimeter in mA measuring mode.
Thanks in Advance.
Diva