Post Go back to editing

EVAL-AD5270SDZ W-PIN Activation Problem

Category: Hardware
Product Number: AD5270

Dear Sir/Madam, 

I am checking A, W-Pin changes using AD5270 EVB.
I think it will be simpler than PWM control of the angle control of the motor, so I'm reviewing it.
50-TP is not used in AD5270 EVB.
When controlled, the signal goes in well. (POWER DOWN - W-PIN level goes down)
There is no W-Pin change according to the register control, so please give me some advice.

< Condition >

1. RDAC direct control 

2. Power is used with AD5270 power on the SDP Board (LK8 PIN - 5V_USB)

3. The AD5270 SPI waveform checked by the IC input terminal is normal.

Best & Regards, 

Mike Noh

Thread Notes