Post Go back to editing

LTC2662 Switch to V- mode

Category: Hardware
Product Number: LTC2662

Hello,

I am using the LTC2662 as a current source to drive a proportional solenoid valve, and here are a few questions I have.

The coil resistance is 500 ohm, and the driving current is 10mA at full opening.

I need to control the current direction in the coil, so is it a good idea to wire the load between OUT0 and OUT1 and use one output in "switch-to-V- mode", while V- is attached to ground ?
In this way, to make the current flow in one direction, OUT1 is in “switch to V-” mode and OUT0 is the current source. And for the opposite direction, OUT0 is in “switch to V-” mode and OUT1 is the current source. See the schematic attached.

Also, for convenience, I would like to use the LTC2672 with VDDx wired to a 5V supply. Unfortunately, that a bit too low to drive the 500ohm load at 10mA even with the low dropout output of this chip.
Is there any circuit that I could add between DAC and load, such as a unity gain current amplifier with low input impedance and high load driving capability ?

Thank you in advance for your help !
Regards

  • Hi  ,

     is currently taking a look at this query and will get back to you. Thanks for your patience.

    Br,

    Den

  • Hi  

    I don't see an issue with the implementation you want to do. Just make sure be careful in setting the modes for each output pin. I suggest you default them to "switch to V-" first before setting the other to output a current. Sort of a break before make sequence, if that makes sense. Also you need to factor in the specs accompanying the switch to V- feature, if you look at table 2 from the datasheet, under DC performance you would see and impedance and a max DC current. 

    The current circuit you have should already work. You would need more than 5V due to drop out, to supply 10mA to a 500 ohm load. 

    You could use any op-amp as a buffer but you have to take into account if the output stage is able to sink 10mA with a only GND level at the negative supply. 

    Best regards,

    Ian

  • Hi  

    Bidirectional currents can be generated using an IDAC and an Analog Switch. For the connections, you can refer to the attached diagrams . The IDAC provides a unidirectional positive current at its output, and the analog switch is responsible for changing the direction of the current in the load.

    For the solenoid value which is inductive in nature, you need a capacitor at the IDAC output to GND to slow down the transition for stability purposes.

    Regards

    Vikash