KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
Could you please advise on any additional troubleshooting steps or potential issues with my current configuration?
Thank you for your support.
Best regards,
Urban


Hi electro633
You need to write first to the control register to disable the write protect. Then execute your write command for the RDAC.
Command: 0x1802
00
0110 - Write serial data to control register
XXXXX - dont cares
0010 - Set DB1, RDAC write protect to allow wiper update
See Table 12 & 13 from the datasheet.
Let me know if this works.
Best regards,
Ian
Dear iandal,
I am sorry to report, that suggestion didn't work. (tried on two PCBs)
I tried various combinations of bits for control register
Ready pin (with pullup) seems to be high the whole time, resistance on both sides of the wiper remains at 10 kOhm
Kind regards, Urban

Dear iandal,
I am sorry to report, that suggestion didn't work. (tried on two PCBs)
I tried various combinations of bits for control register
Ready pin (with pullup) seems to be high the whole time, resistance on both sides of the wiper remains at 10 kOhm
Kind regards, Urban

Hi electro633
During SYNC transition to falling edge, the idle SCLK must be low as mentioned in the timing diagrams.
Regards
Vikash
Thank you, it works now!
Thanks a lot for all the help, much appreciated