Post Go back to editing

DAC output OSCILLATING when combining MULTIPLE CHANNEL

Thread Summary

The user encountered oscillations in the combined output of LTC2672 DAC channels when driving a high-power LED (Cree XML). The issue was partially mitigated by adding a 22uH inductor, but the final solution involved using only decoupling capacitors, a voltage follower for the MUX output, and ensuring a stable power rail. The oscillation amplitude and frequency varied with output current and input voltage.
AI Generated Content
Category: Hardware
Product Number: LTC2672

Hi,

To test the capabilities of the LTC2672, I am using it to drive a high power LED (cree XML). I am combining channels 0 to 3 to allow for a high output current, around 400 to 500mA. The system worked well at first glance, I successfully lit up the LED and was able to adjust its brightness by controlling the DAC channel output current. However, when I looked at the output voltage of the DAC (channels 0 to 3 combined), it was oscillating (see oscillation.png). This does not happen when using only one channel, however, as soon as I link 2 channels together, even if one is powered down, the output voltage is oscillating. The problem was partially solved when I mounted a 22uH power inductor in series between the combined DAC output and my LED. The inductor is able to filter the ripple, because "none" can be observed after it (see. ripple_filtering.png), but the oscillations can still be observed before. The DAC is supplied with VCC=5V, it as to dissipate some power but does not exceed 90 °C which should be okay. Also, I am using the same output span for all channel as advised.

To be sure it wasn't my design causing this, I tried with the development board and observed the same behavior (two channels tied together seems to cause only small oscillations, but the more channel you link, the more oscillations you get). My application will require a great current/voltage stability, is there some recommendations in this case when combining multiple outputs ? Is there some recommendations in terms of ripple filtering ? Have this behavior been observed before ? This phenomenon is surprising considering the datasheet encourage combining the channels. I saw another query about a similar problem with the same component, but it was left unanswered.

Thanks in advance,

Antoine Richard