Post Go back to editing

Is it possible to scale the output up to 8 V with the internal driver and a single-ended, 10 V power supply?

Category: Hardware
Product Number: AD558

The AD558 datasheet describes a couple operating mode for output scaling that provide either 10V full scale, or 2.56 V full scale. The former is not available with VCC lower than 11.4 V (presumably because the output opamp is not rail-to-rail?). Is there a configuration that would increase the full-scale output above 2.56, but lower than the opamp saturation limit? For example, it appears that tieing Vout Select and Vout Sense together and then connecting them to Vout through a 26.3 kOhm resistor would imply an opamp gain of 19.3 for the output stage and a resulting full scale voltage of 8.0 V. Building this in a prototype circuit board results in a much higher gain and saturated opamp behavior.

  • Hi  ,

    Based on the AD558 datasheet specifications, it might not possible to safely scale the output to 8V with a 10V power supply. The device only supports two factory-calibrated ranges: 0V to 2.56V (requiring VCC between +4.5V and +16.5V) and 0V to 10V (requiring VCC between +11.4V and +16.5V). While the datasheet shows a method for minor scale adjustments in Figure 4, the internal resistors have a ±20% absolute tolerance and -50ppm/°C temperature coefficient, making larger scale modifications unreliable. The output stage uses an NPN transistor with passive pull-down architecture, which requires proper VCC headroom for specified operation. To maintain specified performance, you should either use the 2.56V range with your 10V supply.

    Br,

    Den