Hello support team,
I am using AD5754R with FPGA. I have maximize the SCLK to 30.30 MHz. My output range selection is 5 V. I am using LDAC functionality as well. In order to figure out the step response , My SDIN to individual channels are 0000 (Hex) to FFFF(Hex). between SDIN inputs I ma providing 2 clock delays. ( as we have found that by zero clock delay between 2 SDIN Inputs, DAC output is random and not accurate). As the DAC maximum update rate is 1 MSPS and DAC has four channels. Single channel update rate will be maximum of 250 KSPS. But at the output I am getting only 155 KHz with the above mentioned inputs.
Request you to provide feedback and guidance on how to maximize the DAC 5754R update rate. Awaited your quick response.
) per this sentence, once the DAC channel 1 is getting latched it can provide DAC constant output till DAC channel 1 does not get new 24 bit data, right?