Post Go back to editing

How does enabling the 5%overrange affect the transfer function of the AD5761R DAC?

Category: Datasheet/Specs
Product Number: AD5761R

I plan to use the ±3 V range. Will sending the code 0xFFFF output 3.15 V and 0x000 output -3.15 V?

What will the new equation for the transfer function be with overrange enabled?

Parents Reply
  • Apologies for the late reply. Following the datasheet's transfer function equation, for ±3.15V range, M=2.52 and C=1.26.

    The increase in M and C value is also 5%.
    To cross verify the constants, you can try to calculate using 2 equations. First, when Vout = +3.15V (D=65535) and another equation when Vout = -3.15V (D=0).

    Regards,
    Flynn

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.