Post Go back to editing

Question about AD5725 reference voltage

Category: Datasheet/Specs
Product Number: AD5725

From the description from datasheet, it is OK as below

AVdd = +5V, AVss=0, DGND =0V, Vrefp = +2.5V, Vrefn=0V

But Vrefp input range given from datasheet is:

The Vrefp input range: min = Vrefn +2.5V , max = AVdd -2.5V

Then min = 0V + 2.5V = max = 5V - 2.5V, there is no margin.

Any more explanation about it?

Parents Reply Children