I want to use AD5781 in very sophisticated, time-critical project and need your help to understand some things
There is one line in the datasheet which states, "Maximum SCLK frequency is 35 MHz for write mode and 16 MHz for readback mode." on page 5

Here are the queries i have about the SPI Clock,
1. When the DAC is initialized, what will be the starting clock speed? 16Mhz or 35Mhz
2. If the initial clock frequency is 35 MHz, will it only change to 16 MHz when I use the read command?
3. Will the clock continue to run at 35 MHz while writing? unless the read operation is executed.
Your help will be appreciated
Thank you in advance.