Hello,
We are working with AD5545, 16 bit DAC. We have made the proper connection. The AD5545 is configure with SPI with any controller. However the output is not changing by changing the input. Please resolve the issue.
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
Hello,
We are working with AD5545, 16 bit DAC. We have made the proper connection. The AD5545 is configure with SPI with any controller. However the output is not changing by changing the input. Please resolve the issue.
JEstayo - Moved from Precision ADCs to Precision DACs. Post date updated from Monday, June 17, 2024 5:54 AM UTC to Tuesday, June 18, 2024 12:29 AM UTC to reflect the move.
Hi Scientific ,
To help resolve your issue, please provide a schematic, scopeshots of SPI signals, and your SPI configuration details (clock speed, mode, etc.).
Br,
Den
Hi dendalisay,
can you help me to resolve the issue.
Hi Scientific ,
1.) As per checking with the diagram I can see that there's seem to be a data setup and hold time violations (SDI on the 18th bit is on the same edge as the clock). The scopeshot seems to be from a logic analyzer. Can you provide it using an oscilloscope? This way we can check the voltage levels?
2.) Can you clarify as the reference voltage as well?
3.) Another unknown that might be contributing to the issue is the the fact that the LDAC rising while CS is falling.
Best Regards,
Den
hi,
can you provide the waveforms for the same, so I can compare with my waveforms.
Thanks
Hi Scientific ,
You may refer to the timing diagram section of the datasheet. That will provide the proper data setup and hold time specifications that should be observed.
Br,
Den
Hi Scientific ,
You may refer to the timing diagram section of the datasheet. That will provide the proper data setup and hold time specifications that should be observed.
Br,
Den
hi,
we referred the same specification for hold time and setup time.
Thanks
Hi Scientific ,
Kindly try changing SPI modes because as per checking with the attached shots I can see that there's seem to be a data setup and hold time violations (SDI on the 18th bit is on the same edge as the clock)
Br,
Den
hi, i am getting the output range from -1.6 to -3.3 for 3.3 voltage reference. for all input range from 0 to 65535.
Hi Den,
finally, we achieve the output as expected. Thank you for the kind help.
Thanks, and Regards
Rohit Jain