Post Go back to editing

Output is not changing when configure with SPI.

Category: Datasheet/Specs
Product Number: AD5545

Hello,

We are working with AD5545, 16 bit DAC. We have made the proper connection. The AD5545 is configure with SPI with any controller. However the output is not changing by changing the input. Please resolve the issue.

Thread Notes

Parents Reply
  • Hi  ,

    1.) As per checking with the diagram I can see that there's seem to be a data setup and hold time violations (SDI on the 18th bit is on the same edge as the clock). The scopeshot seems to be from a logic analyzer. Can you provide it using an oscilloscope? This way we can check the voltage levels?

    2.) Can you clarify as the reference voltage as well?

    3.) Another unknown that might be contributing to the issue is the the fact that the LDAC rising while CS is falling.

    Best Regards,

    Den

Children
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.