Post Go back to editing

Tolerance in Linear Gain Mode for AD5142A digital potentiometer

Category: Datasheet/Specs
Product Number: AD5142A

Hi, I have checked the datasheet for the ADI542A and have several questions about the Linear Gain Mode:

1. What is the tolerance of R_AW, R_WB and R_AB in Linear Gain Mode?

2. Can we leave W floating in this mode, so it can act like a 20k rheostat? If that is the case, can I ignore the wiper resistance for R_AB?

3. How do you compensate the value with the temperature coefficient? I dont see a formula for it? 

4. The datasheet mentioned the power sequence for VDD first and then A, W and B? Do you know if this implementation will work i.e putting a 1uF across A terminal and ground. 



Edit: I added a 4th question about power sequence
[edited by: CurrentKnguyen at 9:14 PM (GMT -4) on 1 May 2024]
Parents
  • Hi  ,

    1. The tolerance in Linear Gain Mode is disregarded if used as standalone as the tolerance for both Rwb and Rwa are identical. Nominal Resistor Tolerance is the same tolerance for linear gain mode.

    2. Yes, it should ignore the wiper resistance. 

    3. The rheostat temperature coefficient graph can be used for your reference.

    4. That should work given that the Vdd supply connected to the A terminal is also connected to the Vdd pin.


    Best Regards,

    Yokki

  • Hi Yokki,

    Thank you for your reply. 

    I would like to clarify a few things on your response on question #1. From what I understand, the tolerance is disregard if I use R_wa and R_wb as a standalone resistor, so is it within 1% per the graph from AN-1169 below or is it the same as 8% of the nominal tolerance? The application note only specify the tolerance of R_wa whil having a fixed R_wb. Would the tolerance of each resistors change if I want to use them individually? 

  • Hi  ,

    What I meant about "using as a standalone" means there's no external resistor used. One example is when using Rwb and Raw as voltage divider (R1 = Rwb, R2=Raw). The tolerance should be negligible in this case. Figure 14 in AN-1169 however shows that due to the switches inside the part, the mismatch increases as the resistance value of Raw decreases.

    The one you highlighted is referring to a linear response, that is when one resistor is variable, and one is fixed.

    Using them individually, they would have the nominal resistor tolerance, which is 1% typ and 8% min/max.

    Best Regards,

    Yokki

Reply
  • Hi  ,

    What I meant about "using as a standalone" means there's no external resistor used. One example is when using Rwb and Raw as voltage divider (R1 = Rwb, R2=Raw). The tolerance should be negligible in this case. Figure 14 in AN-1169 however shows that due to the switches inside the part, the mismatch increases as the resistance value of Raw decreases.

    The one you highlighted is referring to a linear response, that is when one resistor is variable, and one is fixed.

    Using them individually, they would have the nominal resistor tolerance, which is 1% typ and 8% min/max.

    Best Regards,

    Yokki

Children
No Data