Post Go back to editing

With the same code input to multiple AD5535 sockets, what's the maximum output voltage variation?

Thread Summary

The user asked about the maximum output voltage variation between different units of AD5535 when configured to 5V and loaded with the same code (0x2000). The final answer indicates that the variation should be within the voltage gain spec, which is +/-5% for channel-to-channel gain match error. The user confirmed they meant different units, not channels.
AI Generated Content
Category: Hardware
Product Number: AD5535

For example,

if we configure the output range of AD5535 to 5V, and load the same code like 0x2000 to multiple sockets.

What's the maximum output voltage variation between these sockets?

Parents Reply Children
No Data