I am using AD5592R with a combination of ADC and Three-state channels as follows:
Scenario1:
Channel 0, 1, 2, ... 7 configured as ADC channels: - No problem on ADC sampling.
Scenario 2:
Channel 0, 1, 2, ... 6 configured as ADC channels and channel 7 configured as Three-state - No problem on ADC sampling and also Three-state output channel 7 is working perfectly.
Scenario 3:
Channel 1, 2, ... 7 configured as ADC channels and channel 0 configured as Three-state - PROBLEM on ADC sampling However Three-state output channel 0 is working perfectly.
The problem comes after setting channel 0 to three-state. Then the ADC conversions just keep reading some garbage values, never come ADC sequential values as in scenario 1 & 2.
If I set three-state on any other channel, other than channel 0, then ADC is working perfectly (similar to scenario 2)
Is there anything special on channel 0 setting to three-state resulting ADC sampling to corrupt?
Further to add, no problem on channel 0 three-state and DAC outputs on other channels - the issue seems only with the ADC.