Post Go back to editing

Error rate of capacitor between EXT_CAP and Vss

Thread Summary

The user is experiencing an issue with AD5271 devices in parallel, where some boards become uncontrollable due to capacitors between EXT_CAP and Vss failing in short mode. The final answer suggests checking the capacitance value of the failed capacitors and confirms that the 16V voltage rating should be sufficient. The user's software sequence for updating and reading RDAC values is provided, and the failure is characterized by receiving 0x3FFF at the DIN pin.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD5271

I'm using two AD5271 in pallarell, one for control brightness of LED and one for control sensitivity photo diode.
Datasheet discribes 1uF capacitor should be connected between EXT_CAP and Vss and the voltage rating of capacitor should be ≧7V.

My question is error rate of capacitance.
In my board, both AD5271 has 1uF capacitor between EXT_CAP and Vss, and most of boards works fine, but some boards fell into uncontrolable state of RDAC value, and the capacitor of these boards are corrupted in short-mode.

So I want to know the error rate of capacitance.
If you have any suggestions or information, let me know.

Parents Reply Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.