In my circuit, the DAC LTC2664CUH-12#PBF output is connected to 301ohms series resistor. When the load current of 66uA given at DAC resistor out, i could see a voltage drop at 301 ohms series resistor out side. example: the expected DAC output voltage is 10V. In my board, i could see at DAC IC output, the voltage received is 9.999V but the voltage at 301ohms series resistor out side is 9.9862V when 66uA load current is given at DAC series resistor out. So kindly tell what could be the reason ? have attached the image of the circuit.