Post Go back to editing

Is the maximum output current of the AD5683R internal reference 50 mA?

Thread Summary

The user asked about the maximum output current of the AD5683R's internal reference. The final answer clarifies that the correct value is ±5 mA, as stated in Table 2, and the 50 mA mentioned in the Internal Reference section is a typo. The datasheet will be updated in the next revision.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD5683R

Hello.

I have a question about the internal reference of the AD5683R.

Table 2 "REFERENCE OUTPUT Output Current Load Capability" in the datasheet states ±5 mA.

However, Internal Reference on page 19 states "It is internally buffered and capable of driving external loads of up to 50mA."


Is the maximum output current of the internal reference 50 mA?

Best regards,

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.