Category: Hardware
Product Number: AD5292
Hi Engineers,
I have some questions about configuration and operation of the AD5292. I am looking at using the AD5292 as a VCO tuner for the HMC733LC4B. I would like to control the voltage out of the AD5292 between 21V and 0V. I won't need to daisy chain multiple 5292s nor will I need to use the 20-TP memory register (I think) as just wish to be able to set the RDAC Register after power-up and change the output voltage in a human speed way like a couple times per hour. I would like to know what you all think of the design below. Will it work? If not why and how can I adjust it so it might work?
Thanks for the help.
Caleb