Post Go back to editing

AD5530 INPUT PIN

Category: Hardware
Product Number: AD5530

I would like your advice on AD5530.
My customer is concerned that Vpp (15 V) may appear at the input terminal and destroy the connected output element because the input current (IINH) is stated as ±10 μA(MAX.) in the specification of the input terminal.
I want my customer to use the AD5530 without worry. How should I tell them?

Thank you and best regards,

Top Replies

  • Hi  ,

    The AD5530 has an internal regulator that effectively isolates the digital pins from the 15V power supply. This regulator ensures that the digital pins operate at safe levels of 3.3V.

    Best Regards…

Parents Reply Children
No Data