I have been handed down some MAX11300PMB1 evaluation boards. I have to configure its pins as ADCs to read some voltages from an array. I have tested the eval boards with the Munich GUI and the ADCs seem to work fine (configured as 0-10V) . Now I have to interface it with Arduino over SPI so that I can record the data . But I couldn't find any suitable library, and my programming knowledge is bare minimum. I was hoping somebody could point me to a MAX11300 library and/or a sample code for using its pins as ADCs. I would appreciate the help.