Post Go back to editing

DC590B & DC2692A Msg : Cannot load COM module for the device

Thread Summary

The user encountered a 'Cannot load COM module' error when trying to use the DC590B and DC2692A (LTC2662-16) with QuikEval software on Windows 11. The solution was to run the installed GUI directly instead of through QuikEval, using the 'LTC2662 and Similar' shortcut in the Start Menu. The user confirmed this workaround resolved the issue on a Windows 10 machine.
AI Generated Content
Product Number: DC590B
Software Version: K1117

Just as the original post, I have a DC590B and a DC2692A (LTC2662-16) I'd like to use in conjunction with the QuikEval software. After the initial error message of not being able to load the COM module for the attached device, I found your answer pointing me to the separate download for the driver required for the LTC2662-16. Unfortunately, unlike for the original poster, this did not result in being able to make a connection to the board. It still says 'Cannot load COM module for the device' despite rebooting the machine and executing the QuikEval app with administrator privileges. I would appreciate any additional suggestions on how to make the software work.

Thanks

Parents Reply Children
No Data