Hello,
in our application we intend to use AD5760B DAC for bipolar output +10V/-10V, with the Gain of two. We have 5V as a VREFP voltage, VCC and IOVCC is 3V3. The datasheet says, VREFN is 0V in case of gain of two, I am confused about it, I think that we need also a negative reference voltage -5V on REFN Input. Could you please check the configuration in the picture, is it correct?
Many thanks in advance.
Best Regards.
PS: I also found the application note CN-0318 with +10V/-10V with bipolar reference voltages (VREFP is 10V, VREFN is -10V).