Hi,
I have connected the AD5791 SDZ with the SDP-B controller board and provided a 3.3 V DC voltage supply to the evaluation board (picture 1). Then I have connected the SDP-B with PC via the USB cable and the Device Manager shows a successful connection. It seems to work fine since I get a output voltage at the oscilloscope which is 60V at a power supply of 3.3V which is strange... But somehow I can't use the AD5791 Evaluation Software since I get the message "waiting for transfer to SDP" and it never stops. (picture 2) Also the usb connection seems to be working since when connect it a orange light blinks on the SDP-B controller board.
Picture 2
Picture 1
Thanks for your help.