Category: Hardware
Product Number: AD5421
I've been using the AD5421BREZ for several years. It has always been spot-on 4mA to 20mA over several different board designs with default gain and offset values. Recently, I've gotten some boards back that are now reading 2.1mA to 19.1mA. I was able to increase the offset value to dial in 4mA with 0x0000 DAC, but the offset is maxed out by default and I'm not getting anything over 19.1mA (0xFFFF DAC). The parts appear to be labeled AD5421BREZS1. Boards are the same. I'm not reading any faults. VLOOP is good (24VDC). Load is a 250Ohm precision resistor. How do I make this work?