I am trying to use DEMO 2376A featuring LTC2664-16. Before programming my own controller, I am trying to use it with the Linduino 2026C, which I have purchased as a kit along with DC934A featuring LTC2607.
I managed to use quikeval if using DC934A, it recognizes LTC2607, all fine. Once I connect DEMO 2376A to Linduino, and run again QuikEval K117, it returns "Cannot load COM module for device". I have found on the forum a posting that tells all the module that can be downloaded manually, ins266.msi in my case. Have downloaded, ran it, it created 2 applications: Update LTC2668 and Similar, and LTC2668 and Similar. When running Update... and error message is produced:
If I run then LTC2668 and Similar, the application starts ok
but then:
I click on Reset, then Quit:
then Continue, then the application starts, I enter 2V and Update All, which returns and error message, and clicking Continue does not result in any changes to the outputs of the digital to analog converters.
Please advise.
Daniel
Reviewed post
[edited by: GenevaCooper at 8:38 PM (GMT -4) on 6 Sep 2023]
[unlocked by: GenevaCooper at 8:44 PM (GMT -4) on 6 Sep 2023]