Post Go back to editing

AD5933 Frequency

Thread Summary

The user inquired about AD devices similar to the AD5933 but capable of MHz or GHz output frequencies. The final answer suggested checking the Product Selection Table and seeking recommendations from the High-Speed DACs forum. An accompanying answer noted that the AD5933 can output up to 1 MHz with a 16 MHz external clock, but the 100 kHz limit is due to the built-in low-pass filter. Another engineer recommended the AD9834 for signal generation up to 37.5 MHz.
AI Generated Content
Category: Hardware
Product Number: AD5933

Hi, I noticed that the AD5933 only goes up to 100KHz in output frequency. Are there any other AD devices of similar size and availability that go into the MHz or GHz categories? 

Parents Reply Children