Hi, I noticed that the AD5933 only goes up to 100KHz in output frequency. Are there any other AD devices of similar size and availability that go into the MHz or GHz categories?
Hi, I noticed that the AD5933 only goes up to 100KHz in output frequency. Are there any other AD devices of similar size and availability that go into the MHz or GHz categories?
On 16 MHz external clock the AD5933 can output at up to 1MHz. It is possible to overclock the chip with higher MCLK frequency, the max output frequency scales accordingly (tested it up to 36 MHz MCLK, but this would be off-speck operation, if you choose to do it - all risks are yours alone). The 100 KHz limit comes from the built-in low-pass filter on the receiving side of the chip, not from the excitation.
Hopefully somebody from ADI can help you select some other chips for your application.
Hi jainva ,
Let me double check any products that might be similar and get back to you. For the meantime you may try checking and comparing units using our Product Selection Table.
Best Regards,
Den
Hi jainva ,
Aside from checking our Product Selection Table, let us ask for support with our colleagues in the High-Speed DACs for any ADI product recommendations that is in the MHz or GHz categories.
Best Regards,
Den
Hi Den, was there any luck for ADI product recommendations from the High Speed DACs group?
Hi jainva ,
None yet but I can move this topic to the High Speed DAC forum or you can post similar question there. Additionally you may also try to check our Product Selection Table for highspeed DACs, there you can filter products based on your desired specifications.
Best Regards,
Den
Hi jainva,
For which application is it targeted?
If it is for signal generation, we have DDS that work up to 37.5Mhz such as the AD9834.
Thanks,
Juan.