Post Go back to editing

Does AD9833 need an amplification circuit?

Thread Summary

The user inquires about the necessity of an amplifying circuit for generating a 0V to 5V square wave signal for a test chip. The final answer clarifies that the AD5441 is not a waveform generator but a multiplying DAC that can scale the output of the AD9833. An amplifier is recommended due to the limited driving capability of the digital output, and the AD5451 can be used to scale the VOUT signal, though it may limit the rise time of the square wave.
AI Generated Content
Category: Hardware
Product Number: AD9833

Hi- Everybody

I design semiconductor test equipment.

Therefore, a square wave signal from 0V to 5V must be input to the test chip.

As shown below,

So, do we have to put an amplifying circuit on this chip separately?

Because I saw the following article on the Internet:

" Square wave is reasonably clean/usable up to about 1Mhz. SIN wave is nice and clean up to the max frequency of 12.5Mhz, but the amplitude drops significantly above 1Mhz. This could probably be improved with an opamp with higher gain."

Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.