Post Go back to editing

Doubts about power supply of EVAL-AD5780 board when operated by a microcontroller

Category: Datasheet/Specs
Product Number: EVAL-AD5780SDZ
Software Version: NA

Hi! I am facing a weird situation with regard to powering the EVAL-AD5780 board. As per the user guide UG-256 (RevA),
I need to supply 5 V between the VCC and DGND inputs for the digital supply and 7.5 V to 16.5 V between the VDD and AGND inputs and −2.5 V to −16.5 V between the VSS and AGND inputs for the negative analog supply of the AD5780.

I was supplying +5V for digital and +-15V for the analog and I was completely unable to make the board work. My Links are positioned as follows LK1 - B (external power supply), LK2 - A (+5v), LK3-A (unity gain), LK4,LK5,LK6, removed , LK7 inserted ,LK8 B (AGND) and LK9, LK11 Inserted. As per the instructions, I was always powering on the digital supply before connecting the analog supply. It was not working at all. I was getting +5 at Vref but v_buff_out was flat-out zero regardless of what I sent over SPI. 

However, at one point I accidentally connected the analog supply without the digital one and it started working normally. Now, Basically, Nothing is connected between VCC and DGND. VDD and VSS are connected to =-15 V respectively. And It is working.

My question is, What I was doing wrong, or are the instructions on the user guide wrong? 

Parents
  • The solution to this issue is to connect 3.3 V to the digital supply of the board. The instruction in the user manual on Rev. A | Page 3 of 20 is wrong. It mentions "5 V between the VCC and DGND inputs for the digital supply of the AD5780". This is wrong. If you go above ~3.5/3.6 or below ~2.6/2.7 in digital supply VCC, The circuit will stop working, even if the analog supply VDD&VSS are connected.  

    On the same note and on the same page, in the Connector J3 Pin Descriptions, Pin 5 is mentioned as DGND. It actually labeled as IOVCC on the board. Leave it disconnected. If you give power on it, the circuit stops working. 
      I suggest a update for the user manual of the evaluation board for cases when a SDP board is not used. 

Reply
  • The solution to this issue is to connect 3.3 V to the digital supply of the board. The instruction in the user manual on Rev. A | Page 3 of 20 is wrong. It mentions "5 V between the VCC and DGND inputs for the digital supply of the AD5780". This is wrong. If you go above ~3.5/3.6 or below ~2.6/2.7 in digital supply VCC, The circuit will stop working, even if the analog supply VDD&VSS are connected.  

    On the same note and on the same page, in the Connector J3 Pin Descriptions, Pin 5 is mentioned as DGND. It actually labeled as IOVCC on the board. Leave it disconnected. If you give power on it, the circuit stops working. 
      I suggest a update for the user manual of the evaluation board for cases when a SDP board is not used. 

Children
No Data
More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.