Post Go back to editing

Doubts about power supply of EVAL-AD5780 board when operated by a microcontroller

Category: Datasheet/Specs
Product Number: EVAL-AD5780SDZ
Software Version: NA

Hi! I am facing a weird situation with regard to powering the EVAL-AD5780 board. As per the user guide UG-256 (RevA),
I need to supply 5 V between the VCC and DGND inputs for the digital supply and 7.5 V to 16.5 V between the VDD and AGND inputs and −2.5 V to −16.5 V between the VSS and AGND inputs for the negative analog supply of the AD5780.

I was supplying +5V for digital and +-15V for the analog and I was completely unable to make the board work. My Links are positioned as follows LK1 - B (external power supply), LK2 - A (+5v), LK3-A (unity gain), LK4,LK5,LK6, removed , LK7 inserted ,LK8 B (AGND) and LK9, LK11 Inserted. As per the instructions, I was always powering on the digital supply before connecting the analog supply. It was not working at all. I was getting +5 at Vref but v_buff_out was flat-out zero regardless of what I sent over SPI. 

However, at one point I accidentally connected the analog supply without the digital one and it started working normally. Now, Basically, Nothing is connected between VCC and DGND. VDD and VSS are connected to =-15 V respectively. And It is working.

My question is, What I was doing wrong, or are the instructions on the user guide wrong? 

Parents
  • Hello,

    Please power VDD (analog supply) before powering VCC (digital supply). This is the recommended way of powering up the AD5780.

    If this is a problem, then add a Schottky diode between VDD and VCC as shown in the figure below.

    Regards

  • HI Justlap, Thanks for responding. I am indeed familiar with the paragraph from the AD5780 datasheet. However, as I mentioned, if anything remains connected at VCC and DGND, the chip doesn't work i.e. across V_out_Buff, you don't get any response regardless of what you send over SPI. When you disconnect with VCC and DGND and keep it floating, the chip starts operating as usual. I have not tried with the Schottky diode. I will post the updates next week. 

    But my original question remains the same. Why the chip works only with analog supply but not with digital supply?

  • The AD57809 needs of both supplies, powering them up in sequence, first VDD and then VCC. If my understanding is correct, that's the way you operate the AD5780 without any problem.

    If only VDD is supplied to the part and is still working, that mode of operation must not be used since it can stress unnecessarily internal circuit, current is flowing from VDD to VCC internally instead of being supplied externally via VCC pin.

  • Hi! Sorry for the delayed reply. I understand the standard mode of operation and my original post was about that only. The board doesn't work in that standard mode of operation. Let me elaborate with this example (Simply sending 0 and 262143 with a delay i.e. square pulse) and pictures. Let's Assume Case 1: VDD/VSS supplied with +-15V and VCC is floating. It works Perfectly. Case 2:  VDD/VSS supplied with +-15V and VCC is +5V supplied from the microcontroller, Does not work. Case 3: Disconnect the VCC from +5V supply works again. Connect VCC with a separate power source (Analog Discovery 2) with +5V. Doesn't work again. See the configuration of the Links and the board in the attached picture. 

    With this, please let me know how to address the situation. With the standard mode of operation, the board doesn't work.
    (Sorry your pic upload resolution limit is quite bad. Please find the images at this Photo Link)

  • Two questions:

    Q1: When the AD5780 is powered from the microcontroller or the Analog Discovery, can you please measure the supplies VCC and VDD?

    Q2: Is is possible to capture (using the Analog Discovery analog channels and not the digital ones) the SPI interface, for example clock and SDIN?

  • Hello! Yes. For both of these, I have uploaded the pictures in the same Google Photos folder as before. There is a  comment on the lower right where you can find relevant descriptions. I think it shows that indeed the data is passing over but the chip is not responding when both supplies are connected. 

Reply
  • Hello! Yes. For both of these, I have uploaded the pictures in the same Google Photos folder as before. There is a  comment on the lower right where you can find relevant descriptions. I think it shows that indeed the data is passing over but the chip is not responding when both supplies are connected. 

Children