Post Go back to editing

Is there a SPICE model for AD5246 resistor or it's equivalent (model which works the same but has different ID/name)? Are there even any equivalents for AD5246 from Analog Devices or other manufacturers?

Thread Summary

The user seeks a SPICE model for the AD5246 digital potentiometer or guidance on creating one in MultiSim 14.3. Analog Devices does not provide a SPICE model for the AD5246, but suggests using a single resistor with the same specifications for simulation purposes. The user is implementing a 0V to 30V regulator circuit based on the LM317 documentation, using the AD5246 as a variable resistor.
AI Generated Content
Category: Software
Product Number: AD5246

Like in question, I'm looking for SPICE model of AD5246 resistor or it's equivalent.

If there's nothing like that, would any of you be so generous and describe to me thoroughly the AD5246 functional block diagram so I could design myself component in MultiSim 14.3?

Thanks!

Parents Reply Children
No Data