Post Go back to editing

AD5259_cotrol range

Thread Summary

The user inquires about changing the control range on the AD5259 EVB from 0V to +3.3V or +5.0V. The final answer specifies that for digital inputs, the range is fixed at 2.5V due to the ADG3247 translator, but can be adjusted using an external controller and Vlogic with the A5 jumper set to Vlogic. For Vdd, the A11 jumper should be used to change the range. The user is directed to the EVAL-AD5259 Evaluation Board user guide for more details.
AI Generated Content
Product Number: AD5259

Dear team,

We are reviewing the performance using the AD5259 EVB.

To change the control range from 0V to +3.3V or +5.0V, which value of EVB should be adjusted?

We are looking forward to your advice.

Thank you.

Regards,

Josh

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.