Post Go back to editing

AD5542A VLogic pin

Category: Hardware
Product Number: AD5542A

We are switching from AD5541A to AD5542A in our products due to ic shortages. Our DSP runs at +1.8V. We assumed we could change the voltage at the VLogic pin to run AD5542 with our 1.8v DSP. However, in our tests, we are unable to lower the digital VINH by changing the VLogic voltage. Can you help or provide clarity on why this may be the case?
For our test, we bought an eval board (EVAL-AD5542A), cut the trace on your 2-layer eval board PCB right before the entrance to the Vlogic pin to inject our own logic voltage. (Pretty sure we did a good job in isolating this trace from rest of the board). The voltage at the VL pin is ~4.3 volts by default if no logic input is provided. If we try to inject our own VLogic at a level below 4.3 volts, the +5 VDD and our external power supply for Vlogic start fighting one another. The Vlogic pin seems to work only when the injected logic voltage is higher than roughly +4.3V. This is not how 5541A works and we scanned the datasheet for 5542A to see if there were any differences. We could not find any.
Question: Can we lower VINH by injecting external voltage in AD5542A? If not, why is this input provided?

  • A follow-up question, is it okay to leave Vlogic disconnected?

  • Hi  ,

    Thank you for your patience. As stated on the datasheet, VINH and VINL specs are fixed with the specified VLOGIC and VDD ranges. There is no dependency between VINH and VINL to Vlogic level, unlike the AD5541A. Therefore the AD5542A cannot be run at 1.8V logic level.

    Regarding your question about using an external voltage to adjust the VINH level, this is not possible for the AD5542A as its threshold levels are fixed within the specified VDD range. Additionally, it is important to note that it is never recommended to leave supply pins disconnected as this can affect proper device operation.

    Lastly, we also advise against cutting traces or modifying the evaluation board hardware as it may cause damage and potentially disconnect other devices on the PCB that require VLogic voltage.

    We hope this information helps clarify your questions. If you have any further inquiries or concerns, please do not hesitate to contact us.

    Best Regards,

    Den

More Content

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.