Post Go back to editing

Communication problem with AD5770R

Category: Software
Product Number: AD5770r

SPI communication problem with AD5770R.

I have tried to send records to the card, but when reading them to verify that they have been saved, only zeros (0) are received, which implies that they are not being sent correctly, communication is done through the programmed ESP32 card in the arduino IDE. I have checked the connections and the SPI settings that are set in the datasheet but I am still not able to receive the logs.

Attached code used. The function called “AD5770_start()” is in charge of sending the commands to adjust the card to what is required.

https://drive.google.com/drive/folders/1CILBtWHwDkFTl1--e1I8CDPbe_onu9z-?usp=sharing

Parents Reply Children
No Data