Post Go back to editing

EVAL-AD5676RARDZ Arduino interface using SPI P_MOD pins

Product Number: EVAL-AD5676RARDZ

Hey everyone,

I am new to Analog Eval boards and bought the EVAL-AD5676RARDZ to control 8 channels from the DAC. 

Since it has an Arduino Interface, can I just use it as a shield and attached it on top of a regular arduino? Or is it not compatible and Need the SDP-K1 board?

 

If not, I did solder some leads to the SPI_PMOD  and wired up the Arduino. 

I have pin PMOD_V connected to 3.3V

GND to arduino GND

SCLK to CLK of Arduino pin

SDIN to MOSI line of Arduino pin

and SYNCb to cs from arduino Pin 

I am having trouble sending out the 24 bits of data to the Chip.  I tried following the guide from https://wiki.analog.com/resources/eval/user-guides/dac/eval-ad5676r-ardz

and of course reading the datasheet. 

I Left all the jumper cables as default.

I am powering the P8 pins using the Arduino 5V. 

I am doing a simple command to the eval board.

 

My SPI settings are default. So I just used SPI.begin();

digitalwrite(slaveSelectPin,LOW);

spi.transfer(0x30); //this selects command 0011, and channel VOUT0

Spi.transfer(0xAA); //this is the first 8 bit of the 16 bit value

SPI.transfer(0xAA);  //second set of 8 bits of 16 value

digitalwrite(slaveSelectPin,High);

I chose 0xAAAA as the 16 bit value to easily read from Logic software

I am using the LOGIC Logic analyzer and my timing diagram is way off. 

Any help would be appreciated it. 

Parents
  • Hi  

    We've designed the evalboard to be compatible with most if not all Arduino host boards. Do check the schematic if your host board pinout matches before mounting it as a shield. 

    The hex code 0x30AAAA is correct. Might be your SPI settings, SPI mode. the AD5676R is sampling data at the falling edge of the clock so either SPI mode 1 (CPOL 0 CPHA 1) or SPI mode 2 (CPOL 1 CPHA 0) should work. If this doesn't fix the problem, then try and capture cs, clk and mosi pins on your logic analyzer and we'll have a look. 

    One more debug tip is to check if VREF voltage is available at TP2. SHould be 2.5V

    Best regards,

    Ian

Reply
  • Hi  

    We've designed the evalboard to be compatible with most if not all Arduino host boards. Do check the schematic if your host board pinout matches before mounting it as a shield. 

    The hex code 0x30AAAA is correct. Might be your SPI settings, SPI mode. the AD5676R is sampling data at the falling edge of the clock so either SPI mode 1 (CPOL 0 CPHA 1) or SPI mode 2 (CPOL 1 CPHA 0) should work. If this doesn't fix the problem, then try and capture cs, clk and mosi pins on your logic analyzer and we'll have a look. 

    One more debug tip is to check if VREF voltage is available at TP2. SHould be 2.5V

    Best regards,

    Ian

Children