I have a few issues regarding to AD5593 DAC, for which I need clarification.
First, for DAC pin configuration, pointer byte is: 0000 0101, followed by 0000 0000 and 0000 0001, if I want IO1 as DAC pin. This is clear, isn't it?
For DAC write operation, pointer byte is: D7~D4: 0001 (DAC Write), D3:0, D2~D0: 001 (IO1 pin). For data MSB, D15: 1, D14~D12 (001), the DAC address appears again. Is it correct?
My second question is regarding to ADC conversion, which is illustrated quite clearly in Figure 40.
My question is: if REP bit is not set, and my I2C function tries to read 6 or 8 bytes, are the values from byte 5 to 8 all 0?
Moved to correct forum and added product number tag.
[edited by: emassa at 3:23 PM (GMT -5) on 18 Nov 2022]