Post Go back to editing

Digital potentiometer AD5124 VDD pin connection

Category: Hardware
Product Number: AD5124

Hello,

According to the datasheet of AD5124 we can believe that VDD pin is for biasing "potentiometer staff".

Given that I need to generate voltages in the range -5V ... 0V, can I bias AD5124 in the following way:

  • VDD connect to ground
  • GND connect to ground
  • VSS connect to -5V
  • VLOGIC connect to +5V (or 3.3V)

Thanks.

Parents Reply Children
No Data