Hallo everyone.
My problem is the following: i'm using (on an existing board), an AD5660CRMZ-2 (2.5V ref out) with the supply at 3.3V (instead of 5V typical mentioned in the d.s.).
Basically, i'm supposing to have it as it is and I want to understand the risks
It's not clear to me IF :
- it's a possible choice or there are risks of malfunctions and in case what kind of malfunctions (for example oscillations?)
- Remark:the DAC is used to generate output voltages below 1V; does this fact reduce the criticality?
- the 2.5V internal reference works properly (what is the minimum supply voltage required?)
- does the Ref pin output capacitor size change something?
Best Regards
RC