Post Go back to editing

AD5644 Full Scale Question

Category: Datasheet/Specs
Product Number: AD5644

Hi,

It's not exactly clear from the datasheet if for the external reference case the buffer amplifier still has a gain of 2 as it has in case of using the internal reference(2.5V  for AD5644RBRMZ-5 part and it has a range  from 0-5V).

My system reference is 2.5V too,so will I see close to 5V or close to 2.5V for the maximum scale code?

Also it's a good idea to place a 1nF  decoupling capacitor on the refrence line close to the DAC?

The system reference is buffered at unity gain by an LTC2057  opamp.

Thank you,

Andrei

Parents Reply Children
No Data