Hi,
It's not exactly clear from the datasheet if for the external reference case the buffer amplifier still has a gain of 2 as it has in case of using the internal reference(2.5V for AD5644RBRMZ-5 part and it has a range from 0-5V).
My system reference is 2.5V too,so will I see close to 5V or close to 2.5V for the maximum scale code?
Also it's a good idea to place a 1nF decoupling capacitor on the refrence line close to the DAC?
The system reference is buffered at unity gain by an LTC2057 opamp.
Thank you,
Andrei