Post Go back to editing

The Vlogic pin of the AD5316R is not working

When the AD5316R is connected to VDD=5V, a voltage of 4.25V is automatically generated on the Vlogic. While the I2C pull-up voltage I want to use is 3.3V, Vlogic cannot connect the digital voltage of 3.3V externally, because it will raise 3.3V on the microcontroller power supply.Does the Vlogic have to be supplyed? Will floating affect IC working? If I have to access it, how do I do it?

Parents Reply
  • Hi, 

    The gain pin is categorized as a digital pin, and the max input should be Vlogic +0.3V. If you want to set it high, this should be tied to Vlogic instead. Tying it to VDD has violated the absolute max rating of this pin so I'm not sure if this has damaged the device. 

    Another point is, that you are using the AD5316R, which has an internal reference. I don't see the need to connect the VREF pin to VLOGIC. If you want to use an external reference, I suggest using a reference IC that provides less noise as compared to Vlogic. 

    ~Ian

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.