Post Go back to editing

The Vlogic pin of the AD5316R is not working

When the AD5316R is connected to VDD=5V, a voltage of 4.25V is automatically generated on the Vlogic. While the I2C pull-up voltage I want to use is 3.3V, Vlogic cannot connect the digital voltage of 3.3V externally, because it will raise 3.3V on the microcontroller power supply.Does the Vlogic have to be supplyed? Will floating affect IC working? If I have to access it, how do I do it?

Parents Reply
  • Hi,

    Thank you for your answer. At first, I connected 3.3V to Vlogic pin as power supply, but I found that the 3.3V bus on the MCU was raised to 3.9V during detection. Later, I found that the 3.3V bus was restored only after the Vlogic pin was floating. Therefore, I do not know how to deal with the Vlogic pin, so as to use the AD5316R normally, and does not affect the MCU power supply.

Children