Post Go back to editing

AD5143 maximum AB resistance in linear gain mode

Thread Summary

The user asked if the dynamic range of the AD5143 doubles in linear gain mode, allowing for up to 200 kOhm between terminals A and B when the wiper is left floating. The final answer confirms that the dynamic range is indeed double in linear gain mode.
AI Generated Content

Dear Analog,

If the nominal end-to-end resistance of the AD5143 is 100kOhm in potentiometer mode, does the dynamic range double in linear gain mode? In other words, can I leave the wiper floating and program up to 200 kOhm between A and B ?

Kind regards

Parents Reply Children
No Data